Hi Team,
Does TPS23881 has IEC 62368-1 certificate? If yes, Could you share me the certificate?
Thanks.
Terry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Terry,
We do not have UL certification for TPS23881. Furthermore, we cannot get it at an IC level as our solution is with external FETs.
If UL certification is required, you would have to test it at a system level directly with the UL or just add a fuse on each port.
Best regards,
Sai Gunda