LM3643_TRANS simulation schematic is used as starting point. Pspice model of LM3643 property is modified so that it runs at IR mode. Input DC voltage source is changed from 3.6V to 5V. Pulse th at feeds Strobe pin is V1=0, V2= 3.3, TD=0, TR=10u, TF=10u, PW=8m, PER=10m. Simulation is modified to run for 10ms. I am not sure the what the two LED loads implementation. But simulation result shows, current ILED1 and ILED2 only rise up to 100mA although the LM3643 model set FL1= FL2=0.7A. Please let me know whether this current limit is caused by LED model used. I tried to simulate LM3643 drives two 700mA LEDs or drive LED1 only at 1.4A. Thank you.