Part Number: TPS650864
Other Parts Discussed in Thread: TPS650861
Hi,
Looking at the datasheet, I want to be sure I'm interpreting it properly.
SWVTT_DIS register shows 1 in bit 7, so SWB2 is enabled.
LDOA1_SWB2_CTRL shows 0 in bit 0, so SWB2 is disabled here.
Can you confirm that this means the SWB2 is disabled overall on reset? I think that's what it means.
Also, I think this is more of a formatting question, but why does it say Reset "X" in the table 8-61? Wouldn't that imply an unknown? The same happens in table 8-76.
Thanks,
Darren