This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560430: Can the Fixed Version be Used as Adjustable Version?

Part Number: TPS560430


Dear Sir or Madam,

We would like to use the TPS560430 for a 5.1V output, but couldn't get hold on the adjustable version.

The 3.3V version works in principal, but oscillates. Input voltage is 13.2V. C403 is currently not populated. A value of 220pF did not improve the situation.

Is it possible to adjust the feedback so that the dc/dc converter is stable?

Thanks a lot and all the best,

Heinz