Other Parts Discussed in Thread: TPS2540, TPS2546
We made a TPS2546 to replace the TPS2540. And the Schematic as follow:

When we use TPS2540 the portable device(Meizu note9) can be charged and transmit, the Charging current is 1.39A.
And then we use TPS2546 PIN TO PIN replace TPS2540. The portable device(Meizu note9) can`t charge and transmit.
The R ILIM_HI and R ILIM_LO both are fixed 30K .
To verify that BC1.2 was executed successfully or not, We used an oscilloscope to monitor the waveform of D+ and D- when using TPS2546.

It seems to indicate that BC1.2 successfully shakes hands and chooses CDP mode. But the portable device(Meizu note9) can`t be charged still.