hello expert,
I'd like to make sure the RESIN pin can be open or not.
fig14 circuit seems to show the example of the open case, but I'm confusing the behavior of it.
Seeing block diagram 8.2, RESIN doesn't look to have an internal pull-up or pull-down.
If don't use this pin as another reset signal input, pulling up to Vcc is recommended?
Thank you for your support.
Best Regards,
Kazuki Kitajima