What is the advantage of the high-side driver built into the BQ76942? If it is a low side driver, what are the implications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the advantage of the high-side driver built into the BQ76942? If it is a low side driver, what are the implications?
Hey Jason,
See this application note regarding the use cases for high side FET driving. The main benefit is that high side FETs allow for communication between the microcontroller and the AFE while the FETs are open. https://www.ti.com/lit/an/sluaa84a/sluaa84a.pdf?ts=1660578002545&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FBQ76952
Thanks,
Caleb
Hello, I would like to confirm with you again that when the high-side resistance sampling MOSFET is turned off, the battery can power the AFE and the microcontroller, right? If it is low-side resistance sampling, then after the switches are turned off, the battery can't power them, and they can't communicate, right? Looking forward to your reply, thank you very much.
Hey Jason,
High-side FET control allows communications between the BQ76942 and the Microcontroller to continue even if there is a fault since the ground connections do not separate. When implementing a low side FET configuration, during a fault, the ground connection between the BQ76942 and the Microcontroller becomes disconnected. This does not allow the two devices to communicate with each other.
Assuming you are using one of the regulator outputs on the BQ76942, the FETs being open in either configuration should not affect power delivery to your microcontroller or the BQ76942.
Hope this makes sense. Thanks!
Caleb
Oh, thank you for your help, I basically understand, can I also understand that when the low-side switch is turned off, the BQ76942 can't supply power normally, because the battery may not supply power to it?
Hey Jason,
In both high and low side FET configurations, when the FETs are open, the load will not receive power from the battery. The BQ76942 will remain powered, however.
Thanks,
Caleb