Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI solution against LT8672IDDBM

Other Parts Discussed in Thread: LM74670-Q1, LM74720-Q1, LM74722-Q1, LM74721-Q1

Hi All,

I would like to know whether TI has similar product against the LT8672IDDBM.

This device combine a boost structure for internal power but I think TI do not have such device.

TI's closest device might be LM74670-Q1.

Could you kindly help to check whether you have better suggestion for this part?

Looking forward to your reply.

Thank you.

https://www.analog.com/media/en/technical-documentation/data-sheets/lt8672.pdf 

  • Hi Chia Cheng,

    We have a new family of devices (LM7472x-Q1) very similar to LT8672 with integrated boost Converter (replacing the traditional Charge pump) to drive the MOSFET gate. Please refer to below table for better understanding on differences between LM74720-Q1, LM74721-Q1 and LM74722-Q1

    Feature

    LM74720-Q1

    LM74721-Q1

    LM74722-Q1

    VIN range

    3V-65V

    3V-65V

    3V-65V

    VIN reverse rating

    -65V

    -33V

    -65V

    IQ(on)

    27uA

    27uA

    27uA

    IQ(off)

    1.5uA

    1.5uA

    1.5uA

    Vreg

    17mV

    17mV

    13mV

    Reverse current protection

    response

    0.45µsec

    0.45µsec

    0.45µsec

    Forward turn ON response

    1.9µsec

    1.9µsec

    0.8µsec

    ISO7637 Pulse suppression

    Needs external bi-directional TVS (typically SMBJ36CA)

    TVS-less system design possible

    Needs external bi-directional TVS (typically SMBJ36CA)

    ISO16750, LV124 Compliance

    Yes

    Yes

    Yes

    OV

    Yes

    Yes

    Yes

    Package

    3mmx3mm WSON 12 pin package (compatible with LM74721-Q1)

    3mmx3mm WSON 12 pin package (compatible with LM74720-Q1)

    3mmx3mm WSON 12 pin package

  • Hi Praveen,

    Thank you for the comparison table.

    I will promote our solution accordingly.

    Appreciate your help!