Other Parts Discussed in Thread: LM3405
LED PWM control is being carried out using LM3405A.
Designed to be the same as the application notes in the datasheet.
The diodes are the same, and for C the internal voltage is slightly higher.
Currently, the duty is periodically adjusted using a frequency of 120 Hz, and at this time, high-frequency sound is mainly generated.
What improvements should be made to prevent high frequency sound? (You must use 120 Hz unconditionally.)



And Board A and Board B are designed to have the same LED driver ends, but the output currents of A and B differ by about 10mA.
I don't know why. The only difference is the LM3405A package difference and the number of parallel resistances. Board A used SOT23, two parallel resistors, and one was NC-treated.
Board B used four HVSSOP parallel resistors, and three resistors were NC-treated. I don't know why the current is decreasing...
Do I have to use only one current control resistor?