This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS544B20: default current limit value

Part Number: TPS544B20


Dear team,

I have designed TPS544B20 and set OCP as default value.

According to datasheet, typical value is 26A. May I know the min and max OCP value?

Regards,

Ben 

  •  

    Current Limit Accuracy is listed in the datasheet, +/- 3A

    For a default setting of 26A, the analog trigger point will be 23-29A

  • Hi Peter,

    Are there any factor (like output inductor) will impact the OCP value? 

    I have test OCP from my side and device will trigger to OCP when Iout~=21A

    Regards,

    Ben

  •  

    Proper layout of the AGND to AGNDSNS connections, PGND to System ground connections, and VDD bypass can affect the sensed current.

    Soldering quality of the thermal pad ground connection, which carried the current.

    Stability of the loop, if the loop is not stable and oscillating or generating bursts of 2 or more SW pulses between extended off-times can all increase the sensed current and thus decrease the current limit trip point.

    Also, over heating the IC during reflow can reflow the internal high-temperature die attach and increase the Rdson used for current sense, causing the OCP to trigger early.

    Is the PMBus connected to read the IOUT value?

  • Hi Ben,

    I will close this post as long time no feedbacks. If you need further support, please reply and this post will be open again.