Hello Team,
Good day! We need your help with our customer's concern below.
We use the BQ25886 standalone, works well, except for 2 problems we cannot fix it.
1, If the 5V standard USB-c charger is connected, the STAT pin goes LOW after a lot of delays (more seconds, even more minutes if the circuit is not warmed up.)
2, The battery charging current is sometimes below the configured value and does not charge properly but the STAT pin is LOW. In this case, the only solution is to disconnect and reconnect the USB connector.
Configuration:
Charge current limit: 1.8 A
Input current limit: 2.8 A
Charge voltage: 8.4V (VSET floating)
OTG disabled
The battery pack we tried: 2S3P and 2S2P 7800mAh, 9000mAh.
The issue is independent of USB-c charger type / NTC value, independent from current limit configurations, and independent from battery pack type, all is 8.4V maximum charged voltage.
We cannot figure out what part is responsible for these issues. I attached the circuit diagram with the USB connector wiring.
Please see attachment
Best regards,
Jonathan