This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H000-Q1: output issue

Part Number: TPS4H000-Q1

Hi,

TPS4H000AQPWPRQ1 is a high-edge electronic switching chip. After the diagnostic enabling pin (P11) is pulled up, when the channel is in the OFF state, but the output voltage of OUT1 is 0.47V, and the output voltage of OUT2, OUT3, and OUT4 is 0V. Please help to confirm whether it is normal