This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62085: Schematic review

Part Number: TPS62085
Other Parts Discussed in Thread: TPS54625,

Dear Team,

The Pull-up of Reference PG is recommended to be 1Mohm, because the PG has EN pulled to two LDO & TPS54625,
As a result, the PG of TPS62085 is only 1.43V, which cannot meet the EN =1.6V of TPS54625.
Can the pull-up resistance of the TPS62085 PG pin be changed to 150K?
Is the driving current of the PG the 1mA in the table below?
Thank you~

Many Thanks,

Jimmy