Part Number: TPS784-Q1
Other Parts Discussed in Thread: TPS629203
Hello,
I had some questions on specifics of LDO and Buck's accuracy.
I am trying to compare the accuracy of LDO and buck through lab test.
For LDO, I am using TPS784-Q1 and for Buck, I am using TPS629203.
To be more specific, I am using TPS629203-Q1EVM for buck EVM.
I was looking at the datasheet, but I am confused on which values I should be comparing in order to correctly compare the accuracy.
Resistor tolerance is not included in the LDO's overall accuracy, so I was wondering which values from the datasheets can pair up or match, for the comparison.
TPS784-Q1 (LDO)

TPS629203 (Buck)
![]()

I also had several questions on this matter.
1) In the buck image above, what is the difference between output voltage regulation and feedback voltage regulation?
2) For LDO and buck each, which values should I refer to for the finalized accuracy, with all of the resistor tolerance considered? If it is not shown in the chart above, how can I calculate it with the values above?
3) For this LDO, when the resistor error should be under 1%, what is the output accuracy or regulation for the VSET option and FB option, respectively?
Thank you.