This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51051B: Confused while selecting the Coil

Part Number: BQ51051B
Other Parts Discussed in Thread: TIDA-00318

Hi i am using BQ51051B wireless receiver IC.

But I am confused while selsecting the coil for this one.

I have bought this coil, which is 47uH but I am confused about the values of the components which are to be used.

I have read the datasheet, where in typical circuit diagram the values are calculated according to 16uH.

So please help me calculating the values according to 47uH or please suggest me some other coil which is compatible with this IC.

Regards

Rajbir Singh