Hi team,
I want to use a BJT to control a NMOS. I have a TINA similuation.
Q1, Why AM1 current is a uA current? This uA current is the MOS driver current? How to calculate the mos driver current in this circuit? 5V/100 is the MOS driver current?
Q2, In this circuit, I use 2 BJT to control a NMOS. Is there any way to use only one BJT to control a NMOS?
Q3, When I use another 2 BJT to control the NMOS. If BJT input is 3.3V, NMOS is closed and the IDS of MOS is cloesed to 0. Why NMOS cannot be open? How to improve this circuit?