Other Parts Discussed in Thread: LM3405A
Hi TI,
I'm trying to design a driver for a laser diode and in the chart below you see some test results with TPS54200 and LM3405A. I need to keep the current below 600mA.
Unfortunately the efficiency stays below %77, and as I reduce the current, the efficiency drops further.
This is gonna be hand held device and power dissipation matters a lot.
So I was wondering if you recommend any solution or an alternative converter for a higher efficiency.
540mA current:
|
Vin [V] |
Iin [mA] |
Pin [mW] |
Vo [V] |
Io [A] |
Po [mW] |
Eff. [%] |
|
8.4 |
59.1 |
496.44 |
0.54 |
0.54 |
291.6 |
58.7 |
|
8.2 |
60.2 |
493.64 |
0.54 |
0.54 |
291.6 |
59.1 |
|
8.0 |
61.8 |
494.40 |
0.54 |
0.54 |
291.6 |
59.0 |
|
7.8 |
63.2 |
492.96 |
0.54 |
0.54 |
291.6 |
59.2 |
|
7.6 |
65.0 |
494.00 |
0.54 |
0.54 |
291.6 |
59.0 |
700mA:
|
Vin [V] |
Iin [mA] |
Pin [W] |
Vo [V] |
Io [A] |
Po [mW] |
Eff. [%] |
Laser Temp |
|
8.4 |
285.8 |
2.401 |
2.676 |
0.7 |
1.873 |
78.0 |
30°C |
|
8.2 |
294.8 |
2.417 |
2.677 |
0.7 |
1.874 |
77.5 |
30°C |
|
8.0 |
305.4 |
2.443 |
2.677 |
0.7 |
1.874 |
76.7 |
30°C |
|
7.8 |
311.9 |
2.433 |
2.677 |
0.7 |
1.874 |
77.0 |
30°C |
|
7.6 |
321.8 |
2.446 |
2.678 |
0.7 |
1.875 |
76.6 |
30°C |
|
7.4 |
334.7 |
2.477 |
2.679 |
0.7 |
1.875 |
75.7 |
30°C |
Mamzi