Part Number: TPS23882B
Other Parts Discussed in Thread: TPS23882
Hi Sir,
Does the auto pin of TPS23882B only support af,at? If two pairs of functions, is bt type 3 class 6 supported?
Is there a test report for sifos or EA's bt type 3?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tommy,
The auto pin of TPS23882B is for autonomous mode selection. Any device that supports autonomous mode selection is designated as .bt Type 3. even though power is only provided over 2 pairs. Autonomous mode only has 2 selectable power levels (15W and 30W) therefore any device requesting higher power will be demoted to selected power level.
We have sifos test report for TPS23882, however we do not currently have one for TPS23882B, we can run sifos test on TPS23882B1EVM if needed.
Very Respectfully,
Brandon Beader