Other Parts Discussed in Thread: BQ24610
Hi
Please suggest suitable product to replace LTC4012 LTC4013 LTC4162-L ,Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please describe what features you are looking for so I can better assist you with your search.
Regards,
Mike Emanuel
Hi Michael
Input voltage 26v preferably 40v
Control topology Buck
Chager 1~5 or 6 cells.
Requires Power Path function.
Requires Battery to system power Switch SMBus and Stand-alone two solutions.
Thanks
Hello,
The BQ24616 and BQ24610 offers input voltage up to 28 V. They support up to 26 V battery voltage. They offer connecting the System to the Input when the Input is Present and the System to the Battery when only the battery is present. The topology is Buck.
Regards,
Mike Emanuel