I am designing a new board plan to use TPS552882, the input is 3V-36VDC , and output is 5V, 6A maximum, the Design Calculation temperature rise is around 20degreeC, but Webench warning Design update failed, max junction temperature exceeded. Can I use TPS552882 in this application? Which temperature result is the correct one?