This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: Values for BRT_CONTROL and PWM_OUTPUT_DIAGNOSTICS, EN and INT pins

Part Number: LP8866-Q1

Hello,

This part has been designed into an automotive ECU. My task is to take advange of the LED driver's feature by switching from PWM control to I2C control.

Reading the datasheet, I decided to control the PWM with BRT_CONTROL and to check by reading back BRT_CONTROL (exact value) and PWM_OUTPUT_DIAGNOSTICS (10% PWM deviation accepted).

The components function is further controlled and checked by the EN and the INT pin.

I assume the folling values for operation:

EN set to HIGH     The component is operating

EN set to LOW      The component is in RESET

INT read as HIGH The component has NOT detected a fault

INT read as LOW The component has detected a fault

0%PWM      - LEDs OFF,  values in registers is 0, this is the initial state

50%PWM    -LEDs at half duty, value in register is 32766U

100%PWM  -LED  at full duty, value is register  is 65535U

These are currently my assumptions which I have in my SW development. Are they correct and facts?

Where can I find some example C code?

Thanks,

Florian Rupp