Can you recommend a material with higher overall performance and accuracy than MM3860?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you recommend a material with higher overall performance and accuracy than MM3860?
Hey Jason,
The BQ2980 has a higher OV and UV accuracy than the MM3860. The BQ2980 has a +- 10mV and +- 20mV OV and UV accuracy, respectively. Current consumption for both devices is similar.
Thanks,
Caleb