Other Parts Discussed in Thread: TDA4VM
Circuit: TPS65941111RWERQ1 (datasheet SLVSEA7B – DECEMBER 2019 – REVISED FEBRUARY 2022)
What does the Output filtering effective capacitance actually mean (LDO1-3, chapter 7.5, row 1.1b, LDO4 chapter 7.6, row 2.1b)? Can you load any of the LDO1-4 outputs with more than 4 uF in any case? What do you then risc? What can happen if you load with say 10-20 uF?
When comparing a TI design with the PMIC (TDA4VM Edge AI Kit - DUAL TPS65941x PMICs, PROC112 001 J721EXSKG01EVM, rev A, Monday, October 25, 2021) it looks like for instance the LDO4 of PMIC A is loaded with more than 4 uF. The voltage generated is called VDA_MCU_1V8 and it looks to have at least 2.2 uF + 5*4.7 uF as load. Is that possible (and then why)?