Other Parts Discussed in Thread: TPS61085
Hi,
I have used the TPS61085 in a design to convert 6V to 12V (see below). The EN pin is connected to the microcontroller, with the idea to be able to turn off the output voltage. However, this is not the case. Although the EN signal is LOW, I can measure a voltage of around 5V at the output. I guess it is the input voltage minus the diode drop.
Any good suggestions on how to truly turn off the 12V supply?