This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: ADC Short Circuit Autoss MAXOUT configuration

Part Number: TPS929120-Q1
Other Parts Discussed in Thread: USB2ANY

Hello,

I'm trying to get the autoscan mode to work, but I'm not shure what I am missing.
I want to get the MAXOUT for calculation of the ideal drop to set the output voltage for the prestage (DCDC).
I have the Evalboard here and have this setting:
PWM FREQ = 200 Hz
Auto SS = on
ADC Supply Monitor Threshold = 5 V
ADC Short Detection Threshold = 51
On-Demand Diagnostic Pulse Width = 20 µs
On demand diagnostics Current = 15

I set all channels to on. In the Registermap I set CONF_MISC0 bit for CONF_AUTOSS to 1
Set in CONF_MISC6 the CONF_ADCCH to 5 but the FLAG3 is not updated. do I miss any setting?

Thank you for any help