Hi Team,
When the OVP or UVP protection is active,
Adjust the input voltage to the normal range,
But will keep "auto-recovery" mode and output voltage is not normal.
Need to discharge and reload is required to have a normal output voltage.
Resistor value is correct?
Protect condition is OVP:16.5V and UVP:7.5V
R1=470K
R2=48.7K
R3=41.2K