Hello,
I am an FAE for a distributor that handles TI products.
My customer is considering using the LM73606 with the following specifications.
There is a requirement in the spec that 8000uF be connected to VOUT.
Will this device be okay with such a large capacitance connected to the output?
Are there any concerns in this case?
(Specification)
VIN : 12V (max 36V)
VOUT : 5.1V
IOUT : 6A
Capable of pre-bias operation
8000uF is connected to VOUT
Best regards,