Other Parts Discussed in Thread: TPS65987, TPS65988
Hi, TI Support Team
Inquiries regarding the following applications have been received from customers.
[Monitor that supports USB-C port only]
- Input Signal: Displayport over USB-C
- Input power: 12V (via USB C)
During the review of the application, please answer the following questions about the TUSB564 product.
1. If I design an application using the TUSB564 product, is the TPS65986 (PD controller) applied to the EVM mandatory?
Is it impossible to control through an external MCU?
2. TPS65986 product not found on ti.com.
Is this a discontinued part?
Do I need to replace it with another part?
What items can be replaced?
Please recommend.
Thanks.
Regards,
MJ