Part Number: LP8733
Hello ,
We are using LP87334D for powering up AM243x. Our pre regulator is TPS563210. Please see the schematic attached.
Infact we are getting a 5V output from pre regulator and it is going to LP87334D input. But we are not able to get any output from LP87334D. When we observed what we can see is like the voltage at EN pin and PGOOD is really low (33mV);(EN and PGOOD is shorted). As PGOOD pin is in gated mode of operation in LP87334D(As told in technical reference manual) what I can see from datasheet is that during power up sequence PGOOD will be active (high) upon exiting OTP configuration as initial state and after that for a normal power up sequence PGOOD state is not changed for 800us and it should remain in high state itself as long as output is not going unregulated. But in our case we are not even seeing an high state in PGOOD. Requesting your expertise to suggest what might have went wrong here.
Thanks
Ranjith