This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: can smaller inductor be used?

Part Number: TPS54302


Hi Team, 

can smaller inductor such as 1uH/1.5uH be used?  

I see it is peak current mode, inductor should not affect the loop, so loop compensation should not be the problem. Then is there other limit on reducing inductor if current ripple can be accepted?  

Also, the cap should be limited due to loop, right? but if inductor is smaller, we may use larger Cout to reduce Vout ripple, how to choose the Cout ?  maybe I need to know the position of internal zero. Thanks. 

BRs

Given