This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: How to write the golden image file without using EV2400 and BQStudio

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400

Hi,

Could you tell me How to write the golden image file without using EV2400 and BQStudio?
I can use EV2400 to create the golden image file, but cannot use it to write the file at production.
In my system at production, data is sent from the PC to the CPU using UART communication, and FLASH DATA and calibration commands are sent from the CPU to FUELGAUGE via I2C, see QA_220901.xlsx.
How do I write all the data in the golden image file?

Best,
Hirota
QA_220901.xlsx