Regarding to SLUUAH7B TaperRate = DesignCapacity/(0,1*TaperCurrent). Also a tolerance of 15% is added to the Taper Current in the example.
My charger theoretically quits at 13,3 mA. Logs of the Fuel Gauge show a minimal AverageCurrent of 17 mA before dropping to zero.
I've tested Taper Rate = 96 and 75. At both values the SOC reaches 100 % to early while charging. At Taper Rate = 96 the SOC reaches 100 % around 15 minutes before the charging current drops to zero. At Taper Rate = 75 this seems to happen even earlier.
How do I choose the Taper Rate correctly?