This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
I understood sync. can be easily achieved as follows.
Customer wants to create other situation as follows.
Is it possible to come true?
Tsushima-san,
If using an external clock, the synchronization function is easy and straight forward as you already know from this E2E post you referenced. If synchronizing two TL594 controllers, the same theory can be applied but you need to split the synchronization signal into two separate clock signals operating out of phase with respect to one another. For synchronizing two power stages, this is commonly done at 180° phase shift but you can shift the two signal with any amount of phase shift, such as 45° as you've suggested.
Regards,
Steve M
Hi Steven-san,
So you mean that additional circuit like comparator etc. is essential to be phased shift triangle wave from CT pin,
and cannot achieved phase shift except for 180° w/ just two tl594.
Is this understanding correct?
BR,
Koki Tsushima
Hi Steven-san,
So you mean that additional circuit like comparator etc. is essential to be phased shift triangle wave from CT pin,
and cannot achieved phase shift except for 180° w/ just two tl594.
Is this understanding correct?
BR,
Koki Tsushima
Tsushima-san,
Shown below is an example of 2 clock signal phase shifted by 180° but your external synchronization clock circuit needs to be able to phase shift two signals by 45°
Regards,
Steve