Other Parts Discussed in Thread: TUSB216, TUSB321AI, TUSB542, TUSB542EVM, TUSB522P, TUSB1002A
Hello TI experts,
My customer made their own PCB with TUSB1044, and they have some problems.
Please review the schematic first ;
- host side is connected to PC, and target side is connected to USB storage.
the problem is, if the connector is connected as flipped, USB 3.0 connection is disabled. (USB 2.0 is connected.)
if the connector is connected as not flipped, USB 3.0 connection is okay.
is there any way to detect flip status in host side?
and here are more questions.
1. is there any output pin which is same as CD pin in TUSB1044? (the screenshot below is about TUSB216.)

2. is there any way to reset TUSB1044 externally (like EN pin)?
Please check these issues. Thanks.
Best regards,
Chase