This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FLYBUCK-FLYBACK-DESIGN-CALC: Design for 100W DC/DC Flyback

Part Number: FLYBUCK-FLYBACK-DESIGN-CALC
Other Parts Discussed in Thread: LM5155, LM5156
Hello, We are wondering if there is any suitable controller and circuit or calculator for the design of a flyback topology DC/DC converter that can meet the requirements below?

DC Input : 12V,typ (+/-5%)

Output Power : 100W

Output : 310 v – 330V

Regards