This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200-Q1: This chip can meet the requirements of input 5V, output 4V/2.5A buck, 100% duty cycle, 1mA light load efficiency of about 90%? Is there a more suitable recommendation?

Part Number: TPS40200-Q1


This chip can meet the requirements of input 5V, output 4V/2.5A buck, 100% duty cycle, 1mA light load efficiency of about 90%?

Is there a more suitable recommendation?