I need clarification in part difference for TPS54561 and TPS54561-Q1.
From datasheet i could find following difference,
Parameter | TPS54561-Q1 | TPS54561 |
ESD rating | Automotive AEC-Q100 AEC Q100-002 indicates HBM stressing is done in accordance with the ANSI/ESDA/JEDEC JS-001 specification. |
Catalog Human body model: (1) JEDEC document JEP155 states that 500-V HBM allows safe manufacturing with a standard ESD control process. Charged device model: (2) JEDEC document JEP157 states that 250-V CDM allows safe manufacturing with a standard ESD control process. |
Shall i use TPS54561 part as a replacement for TPS54561-Q1. Is there any other difference other than the above point and please elaborate the ESD qualification (Automotive and Catalog)