This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: Can the LM5146-Q1 IC be used as fly-buck converter?

Part Number: LM5146-Q1
Other Parts Discussed in Thread: LM5146, LM5160, LM5160-Q1, LM25184

LM5146-Q1 meets the following requirements to be used as a fly-buck.

1. Synchronous rectification.

2. Diode emulation feature at light loads can be turned off. 

My requirements are as follows: Gate drive application (HV  Inverter)

Input 10-18V 

6 isolated outputs: Three 15V and Three -8V (each output at 100mA)

Non isolated output may be +5V or any other voltage.

Just wanted to confirm if it can be used?

Please provide a reference schematic for the same.

Thanks!