This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25143-Q1: LM5143DESIGN-CALC question

Part Number: LM25143-Q1


Hi,

The customer wants to use LM25143-Q1.

Spec 1 : Dual Output 

Input Voltage : 21~27V

1Ch Output Voltage : 12.5V

1Ch Output Current : Max 30A ( Typ 25~27A )

2Ch Output Voltage : 12.5V

2Ch Output Current : Max 30A ( Typ 25~27A )

Spec 2 : Single Output

1Ch Output Voltage : 12.5V

1Ch Output Current : Max 30A ( Typ 25~27A )

Q1. Can use it with 2 specifications?

Q2. Or, please recommend a product that meets the single output specification.