This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360: Two of this device in parallel?

Genius 17405 points
Part Number: TPS54360

Hi Experts,

Is it okay to use two TPS54360 device to increase the load capacitance by parallel output terminals. Such a design, two outputs directly connected to one side and then to the load side, does it have any impact?

Thank you.

Regards,
Archie A.

  • Hi Archie, 

    Two TPS54360 devices cannot be easily paralleled to evenly share the total power.  An external sharing control circuit is needed.  You may refer to the concept in Figure 4 of the following App Note to force the two circuits to evenly share the total power.  Note that you may consider to provide external clock to synchronize the two circuits in order to avoid the noise at the beat frequency.

     https://www.ti.com/lit/pdf/snva826

    Thanks,

    Youhao

  • Because there is no update for more than a week, may I assume the issue has been resolved and close the thread here?  You are welcome to re-open it by adding a new post. 

    Thanks and good luck in your project.

    Youhao