Other Parts Discussed in Thread: UCD90320
Hi there
What does external ADC reference voltage do ?
Does it relate to AMON pins?
It means that AMON pin can not accept voltage higher than 3.0V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mike, this is really a UCD90320 question. While I am familiar with the UCD3020, I can't translate this knowledge to the UCD90320 because the pinout is different, and the pin names are different, and I'm not familiar with the programming of the 90320. For future questions, please refer to the 90320. I'm going to forward this to the 90320 application engineers.