This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3020: UCD90320 HW schematic revew

Part Number: UCD3020
Other Parts Discussed in Thread: UCD90320

Hi there

According to customer feedback, we run reboot cycle testing it causes  UCD90320  "dead".

Could you help to review our schematic for A1/A2

A1_UCD90320_1.pdfA2_UCD90320_1.pdf

Thanks

Mike Hsu

  • This is an urgent please check asap

  • Hi

    what kind of reboot cycle testing it is? could you provide more details?

    What do you mean dead? does a reset(toggle the reset signal) bring the UCD90320 out of dead?

    Schematics look fine.

    Regards

    Yihe

  • what kind of reboot cycle testing it is? could you provide more details?

    Ans: the customer was running the reboot with PDU.

    What do you mean dead? does a reset(toggle the reset signal) bring the UCD90320 out of dead?

    Ans: We found I2C can not communicate it anymore, and RESET pin (G10) has 300 ohm resistance (before was 800 ohm)  from P3V3_DPM to GND. We believe there is an internal damage in the IC. 

    Q1: Is there power ON / OFF and RESET timing requirement for UCD90320 IC?

    Q2: Have TI or other customers experience this issue before? If yes, what is the root cause?

    Q3: We will send the damaged IC for more detailed analysis.

    Mike Hsu 

  • Hi

    what's the frequency between reboot?  are stress tested done between reboot?

    Are both UCD90320 dead? Did you probe the SYNC_CLK(K2) pin to see whether it has clock output? if it does have 5KHz clock, the device is alive. 

    What's the voltage of V33A, V33D, BPCAP and RESET when the device is dead?

    1. No

    2. No

    3. how many units are failed? what's the percentage?

    Regards

    Yihe

  • what's the frequency between reboot?  are stress tested done between reboot?

    Ans: PDU was first turned ON and running stress test for 30 minutes, and then turned PDU off for 5 seconds, and turned ON again (AC power cycle)

    Are both UCD90320 dead? Did you probe the SYNC_CLK(K2) pin to see whether it has clock output? if it does have 5KHz clock, the device is alive. 

    Ans: One UCD90320 per PCB. The defected board has sent to Taiwan, we will measure it when we received board

    What's the voltage of V33A, V33D, BPCAP and RESET when the device is dead?

    Ans: The defected board has sent to Taiwan, we will measure it when we received board. 

    How many units are failed? what's the percentage?

    Ans: There is only one failed out of 3 boards.

    My another question is what if GPIO pin pull up voltage is ealier than V33D, what is the risk? what is the initial state of these GPIO?

    Thanks

    Mike Hsu

  • Hi

    it is up the current since if the GPIO is power up the internal esd diode maybe active

    the best is to measure the failed unit 

    regards

    yihe

  • Hi Yihe

    According to TI document SLVUB50C, when the IC is in RESET# or INITIAL state, its GPIO pins are in Hi-Z. So I don't think current or voltage can damage the GPIO pins.

    Thanks

    Mike 

  • Hi

    It is different, under RESET or INITIAL UCD90320 is already power up.

    but what you said in the early post is that GPIO is pull-up early than V33D. it means that the GPIO has voltage before UCD is power up.

    Regards

    Yihe

  • Hi Yihe

    After the measurement, we would like to send the failed IC for further inspection.

    Whom and what address I shall send to?

  • Hi

    Please contact your local TI support team for the FA request.

    Could you share the measurement of the requested data here?

    Regards

    Yihe

  • Hi there

    Following is the resistance between signal pin to GND and siganl to V33D power.

    As you see reset# pin of normal board is 13.2M ohm to GND, but the fail board became 281 ohm to GND.

    V33D power pins to GND resistance is relatively smaller than normal board. ( 185 ohm VS 812 ohm)

    Singal Board To GND To P3V3
    DPM_RST_L Fail(Remove R186 and C121) 281 465
      normal 10.8k 10k
      Normal(Remove R186 and C121) 13.2M O.L.
    P3V3(V33D) Fail(Remove R186 and C121) 185  
      normal 812  
    DPM_BPCAP Fail(Remove R186 and C121) 10.3k  
      normal 10.5k  
    DPM_V33A Fail(Remove R186 and C121) 186  
      normal 808  
  • HI

    Have you powered up the returned unit to check the voltage(V33, Reset, BPCAP)?

    Regards

    Yihe

  • Hi

    No, because we do not want to do futhur damage.

    It's very clearly that something  not right.

  • HI

    Sure, Understand the concerns.

    We will process once the part is received. Please ship a control unit as well.

    Regards

    Yihe

  • Sorry 

    We can only provide failed UCD90320 due to NDA 

    How quickly TI takes to anaysis this IC?

    This is a very urgent issue

    Thanks

    Mike Hsu

  • Hi

    For a typical FA, it is always good to provide a control unit along with failed unit to check.

    Please contact your local TI support to start the FA.

    I am going to close this post.

    Regards

    Yihe

  • Hi Yihe

    We found another fail piece after AC ON/OFF stress test yestarday. 

    1. Can you check A1 & A2 schematic again that I attached in this session. I found unused GPIO pin should connect to GND according to https://www.ti.com/lit/ug/slvub50c/slvub50c.pdf

    2. Is there power up / down timting between RESET_N pin and V33D power rail?

    3. An AMONx pin is connected to ATX 12V with voltage divder circuit. This AMONx pin get  ATX 12V before V33D and RESET_N pin change to high. Will this AMON pin get damaged? 

    PS. UCD90320 does not enable ATX 12V

    Thanks

    Mike Hsu

  • Hi

    Even leaving GPIO floating, i can not think how it can damage the silicon unless there was some spike on the pins. We recommend 4.99ohm between V33D and V33A, but you have 0ohms there.  Even so, i do not expect it causes problem.

    What is difference between P3V3 and P3V3_DPM? i saw you have different nets for the supply. 

    Powering up AMON before supply could lead to a leakage, but you have the current limitation resistor on that AMON to reduce the current. which pin is it?

    is your test always under Room temp?  will be any soldering issue have your run x-ray?

    Regards

    Yihe

  • 1. P3V3 =  P3V3_DPM is the same power rail. Both them are connected together.

    2.  AMON2 (E1) is connected to ATX 12V.

    3. Yes, it was tested under room temperature. X-ray looks fine and flying probe was tested as well. No issue was found.  

    4.  Is there power up / down timting requirement between RESET_N pin and V33D power rail?

  • Hi

    Your reset design is good. where is the RST_L from?

    Regards

    Yihe

  • Hi

    RST_L does not connected to outside, it only connects to UCD90320 RESET_N (G10) pin.

    Therefore, RESET_N became de-assert after P3V3_DPM power up.

  • Hi

    I do not see any problem on the reset. Maybe there are something on the layout?

    Regards

    Yihe

  • I applied for CPR (Product return: CPR221071120)

    Quality Tracking Number: QEM-CCR-2210-00001

    This issue is point to EIPD (Electrically Induced Physical Damage) according to TI's response. However my question is can TI provide more information on absolution maximum rating for negative input voltage? For example. tolerance on negative voltage, time before damage.

    What is TI suggestion to reduce negative voltage?

    We have found abnormal waveform with some PSU that the negative voltage > -0.3V during power on.

    Thanks

    Mike Hsu

  • Hi

    Negative voltage is not supported on the power supply pin. for the IO pins, the -0.3V is the lowest to go.

    But please be understood that operation outside of the absolute maximum ratings can damage device and host shall avoid any kind of situation 

    Regards

    Yihe