Other Parts Discussed in Thread: 4428, BQSTUDIO
To whom it may concern:
We are trying to use the Fast_QMAX_FLD function, in order to update the MAXERROR in the field use. Based on our tests, the QMAX update is not really consistent.
1st test: battery fully charged, rest for 30mins, fully discharge the battery, and QMAX updated right after discharging, as expected, MaxError = 1% (which means RA table updated as well)
2nd test: same conditions as above, but MaxError didn't update and kept as 6%. So QMAX didn't update.
3rd test: after charging rest for 2hrs, and fully discharge the battery; QMAX didn't update
4th test: regular QMAX update condition, after charging rest for 2hrs, after discharging rest for 5hrs, QMAX didn't update
5th test: repeat 4th regular QMAX update condition, QMAX updated.
In order to observe the MAXERROR update, the Max Error Time cycle equivalent is set to 1, and Cycle Delta is set to 1 as well. One of the battery shows abnormal MAXERROR as 101%, and could update to 74% or similar. Is this a bug? The full log file is too large to attach here.
Sample | DateTime | ElapsedTime | ManufAccess | RemCapAlarm | RemTimeAlarm | BattMode | @Rate(@) | @TimeFull | @TimeEmpty | @RateOK | Temperature | Voltage | Current | AvgCurr | MaxErr | RSOC | ASOC | RemCap | FullChgCap | RunTimeEmty | AvgTimeEmty | AvgTimeFull | ChgCurr | ChgVolt | BattStat | CycleCnt | MaxTurboPwr | SusTurboPwr | MaxTurboCurr | SusTurboCurr | SoH | OpStatA | OpStatB | TempRange | ChgStat | GaugeStat | ITStat | MfgStat | SafetyAlertAB | SafetyStatAB | SafetyAlertCD | SafetyStatCD | PFAlertAB | PFStatAB | PFAlertCD | PFStatCD | CellVolt1 | CellVolt2 | CellVolt3 | CellVolt4 | vBAT | vPACK | CellCurr1 | CellCurr2 | CellCurr3 | CellCurr4 | CellPower1 | CellPower2 | CellPower3 | CellPower4 | Power | AvgPow | IntTemp | TS1Temp | TS2Temp | TS3Temp | TS4Temp | CellTemp | FETTemp | GaugeTemp | FltRemQ | FltRemE | FltFullChgQ | FltFullChgE | NoLoadRemCap | TrueRemQ | TrueRemE | InitialQ | InitialE | TrueFullChgQ | TrueFullChgE | T_sim | T_ambient | RaScale1 | RaScale2 | RaScale3 | RaScale4 | CompRes1 | CompRes2 | CompRes3 | CompRes4 | PackGrid | LStatus | CellGrid1 | CellGrid2 | CellGrid3 | CellGrid4 | StateTime | DOD0_1 | DOD0_2 | DOD0_3 | DOD0_4 | DOD0 Passed Q | DOD0 Passed E | DOD0 Time | DODEOC_1 | DODEOC_2 | DODEOC_3 | DODEOC_4 | QMax1 | QMax2 | QMax3 | QMax4 | QMaxDOD0_1 | QMaxDOD0_2 | QMaxDOD0_3 | QMaxDOD0_4 | QMaxPassedQ | QMaxTime | Tk | Ta | RawDOD_1 | RawDOD_2 | RawDOD_3 | RawDOD_4 | CBTime1 | CBTime2 | CBTime3 | CBTime4 | CBDOD_1 | CBDOD_2 | CBDOD_3 | CBDOD_4 | CBTotalDODChg | SOH_FC_Q | SOH_FC_E | LogRowTime(ms) | LogStatus |
1 | 9/3/2022 8:09 | 4.008 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 24.1 | 11473 | 4114 | 1234 | 101 | 67 | 63 | 4494 | 6786 | 65535 | 65535 | 122 | 4000 | 12300 | 0x0080 | 13 | -19375 | -13739 | -22794 | -14400 | 93 | 0x0187 | 0x1000 | 0x04 | 0x0004 | 0x90 | 0x0D18 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3809 | 3853 | 3815 | 0 | 11465 | 11497 | 4109 | 4113 | 4118 | 0 | 1565 | 1585 | 1571 | 0 | 4722 | 1626 | 21.9 | 24.2 | 24 | 196.4 | 196.4 | 24.2 | 21.8 | 24.2 | 4496 | 4706 | 6786 | 7389 | 4679 | 4428 | 4647 | -393 | -475 | 6676 | 7246 | 24.2 | 22.6 | 1000 | 1000 | 1000 | 0 | 27 | 34 | 29 | 0 | 4 | 14 | 4 | 4 | 4 | 0 | 4 | 2082 | 2086 | 2085 | 0 | 2641 | 3074 | 26 | 2848 | 2784 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 5079 | 5112 | 5073 | 0 | 1071 | 1136 | 2.02 | 12962 | 1824 | 1824 | 1824 | 0 | 397 | 0 | 530 | 0 | 1824 | 1824 | 1824 | 0 | 19216 | 6700 | 7304 | 1051 | SUCCESS |
2 | 9/3/2022 8:09 | 8.009 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 24.2 | 11487 | 4115 | 1926 | 101 | 67 | 63 | 4499 | 6786 | 65535 | 65535 | 108 | 4000 | 12300 | 0x0080 | 13 | -19375 | -13739 | -22794 | -14400 | 93 | 0x0187 | 0x1000 | 0x04 | 0x0004 | 0x90 | 0x0D18 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3813 | 3858 | 3820 | 0 | 11477 | 11514 | 4110 | 4123 | 4125 | 0 | 1567 | 1591 | 1576 | 0 | 4730 | 2371 | 22.5 | 24.2 | 24 | 196.4 | 196.5 | 24.2 | 22.5 | 24.2 | 4501 | 4711 | 6786 | 7389 | 4683 | 4433 | 4653 | -393 | -475 | 6676 | 7246 | 24.2 | 22.6 | 1000 | 1000 | 1000 | 0 | 27 | 34 | 29 | 0 | 4 | 14 | 4 | 4 | 4 | 0 | 8 | 2082 | 2086 | 2085 | 0 | 2636 | 3068 | 27 | 2848 | 2784 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 5079 | 5112 | 5073 | 0 | 1066 | 1137 | 2.02 | 12962 | 1824 | 1824 | 1824 | 0 | 393 | 0 | 526 | 0 | 1824 | 1824 | 1824 | 0 | 19216 | 6700 | 7304 | 1083 | SUCCESS |
3 | 9/3/2022 8:09 | 12.014 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 24.2 | 11501 | 4117 | 2452 | 101 | 67 | 63 | 4504 | 6786 | 65535 | 65535 | 104 | 4000 | 12300 | 0x0080 | 13 | -19395 | -13743 | -22818 | -14400 | 93 | 0x0187 | 0x1000 | 0x04 | 0x0004 | 0x90 | 0x0D18 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3818 | 3862 | 3824 | 0 | 11490 | 11527 | 4107 | 4117 | 4119 | 0 | 1568 | 1590 | 1575 | 0 | 4736 | 2938 | 22.9 | 24.2 | 24 | 196.4 | 195.6 | 24.2 | 22.9 | 24.2 | 4505 | 4717 | 6786 | 7389 | 4688 | 4438 | 4658 | -393 | -475 | 6676 | 7246 | 24.2 | 22.6 | 1000 | 1000 | 1000 | 0 | 27 | 34 | 29 | 0 | 4 | 14 | 4 | 4 | 4 | 0 | 12 | 2082 | 2086 | 2085 | 0 | 2631 | 3063 | 27 | 2848 | 2784 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 5079 | 5112 | 5073 | 0 | 1061 | 1137 | 2.02 | 12962 | 1824 | 1824 | 1824 | 0 | 389 | 0 | 522 | 0 | 1824 | 1824 | 1824 | 0 | 19216 | 6700 | 7304 | 1065 | SUCCESS |
4 | 9/3/2022 8:09 | 16.015 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 24.2 | 11511 | 4116 | 2852 | 101 | 67 | 63 | 4508 | 6786 | 65535 | 65535 | 97 | 4000 | 12300 | 0x0080 | 13 | -19402 | -13745 | -22826 | -14400 | 93 | 0x0187 | 0x1000 | 0x04 | 0x0004 | 0x90 | 0x0D18 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3823 | 3869 | 3830 | 0 | 11501 | 11534 | 4116 | 4114 | 4114 | 0 | 1574 | 1592 | 1576 | 0 | 4743 | 3371 | 23 | 24.2 | 24 | 196.4 | 196.5 | 24.2 | 23.1 | 24.2 | 4510 | 4722 | 6786 | 7389 | 4693 | 4442 | 4663 | -393 | -475 | 6676 | 7246 | 24.2 | 22.6 | 1000 | 1000 | 1000 | 0 | 27 | 34 | 29 | 0 | 4 | 14 | 4 | 4 | 4 | 0 | 16 | 2082 | 2086 | 2085 | 0 | 2627 | 3058 | 27 | 2848 | 2784 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 5079 | 5112 | 5073 | 0 | 1057 | 1137 | 2.02 | 12962 | 1824 | 1824 | 1824 | 0 | 385 | 0 | 518 | 0 | 1824 | 1824 | 1824 | 0 | 19216 | 6700 | 7304 | 1046 | SUCCESS |
5 | 9/3/2022 8:09 | 20.03 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 24.2 | 11519 | 4117 | 3156 | 101 | 67 | 63 | 4513 | 6786 | 65535 | 65535 | 93 | 4000 | 12300 | 0x0080 | 13 | -19416 | -13748 | -22842 | -14400 | 93 | 0x0187 | 0x1000 | 0x04 | 0x0004 | 0x90 | 0x0D18 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3823 | 3868 | 3829 | 0 | 11509 | 11544 | 4113 | 4122 | 4113 | 0 | 1572 | 1594 | 1575 | 0 | 4743 | 3700 | 23.3 | 24.2 | 24 | 196.4 | 195.2 | 24.2 | 23.3 | 24.2 | 4515 | 4728 | 6786 | 7389 | 4697 | 4447 | 4669 | -393 | -475 | 6676 | 7246 | 24.2 | 22.6 | 1000 | 1000 | 1000 | 0 | 27 | 34 | 29 | 0 | 4 | 14 | 4 | 4 | 4 | 0 | 20 | 2082 | 2086 | 2085 | 0 | 2622 | 3052 | 27 | 2848 | 2784 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 5079 | 5112 | 5073 | 0 | 1052 | 1137 | 2.02 | 12962 | 1824 | 1824 | 1824 | 0 | 381 | 0 | 514 | 0 | 1824 | 1824 | 1824 | 0 | 19216 | 6700 | 7304 | 1048 | SUCCESS |
8988 | 9/3/2022 18:09 | 36014.44 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.5 | 11590 | -3999 | -3999 | 101 | 93 | 85 | 6070 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26260 | -15134 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3880 | 3837 | 3873 | 0 | 11578 | 11551 | -4004 | -4004 | -4003 | 0 | -1554 | -1536 | -1550 | 0 | -4634 | -4637 | 27.9 | 25.5 | 25.1 | 195.6 | 196.1 | 25.5 | 27.9 | 25.5 | 6069 | 6485 | 6588 | 7145 | 6412 | 6055 | 6451 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 837 | 2029 | 2044 | 2031 | 0 | 930 | 1096 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 930 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1039 | SUCCESS |
8989 | 9/3/2022 18:09 | 36018.46 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.5 | 11588 | -3999 | -3999 | 101 | 93 | 85 | 6066 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26260 | -15134 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3880 | 3836 | 3872 | 0 | 11574 | 11551 | -4003 | -4005 | -4001 | 0 | -1553 | -1536 | -1549 | 0 | -4635 | -4637 | 27.9 | 25.5 | 25.1 | 195.6 | 196.4 | 25.5 | 28 | 25.5 | 6064 | 6480 | 6588 | 7145 | 6408 | 6051 | 6446 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 841 | 2029 | 2044 | 2031 | 0 | 934 | 1101 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 934 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1043 | SUCCESS |
8990 | 9/3/2022 18:09 | 36022.47 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11585 | -3999 | -3999 | 101 | 93 | 85 | 6061 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26251 | -15130 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3879 | 3836 | 3871 | 0 | 11573 | 11549 | -4003 | -4003 | -4001 | 0 | -1553 | -1536 | -1549 | 0 | -4633 | -4636 | 27.9 | 25.5 | 25.1 | 196.4 | 196.1 | 25.6 | 27.9 | 25.6 | 6060 | 6474 | 6588 | 7145 | 6403 | 6046 | 6440 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 845 | 2029 | 2044 | 2031 | 0 | 939 | 1107 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 939 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1075 | SUCCESS |
8991 | 9/3/2022 18:09 | 36026.48 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11584 | -3998 | -3999 | 74 | 92 | 85 | 6057 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26251 | -15130 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3878 | 3835 | 3871 | 0 | 11572 | 11546 | -4000 | -4003 | -3999 | 0 | -1551 | -1535 | -1548 | 0 | -4632 | -4635 | 28 | 25.5 | 25.1 | 195.9 | 196 | 25.5 | 28 | 25.5 | 6055 | 6469 | 6588 | 7145 | 6399 | 6042 | 6436 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 849 | 2029 | 2044 | 2031 | 0 | 943 | 1111 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 943 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1096 | SUCCESS |
8992 | 9/3/2022 18:09 | 36031.32 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11587 | -4000 | -3999 | 74 | 92 | 85 | 6051 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26245 | -15127 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3878 | 3835 | 3870 | 0 | 11571 | 11545 | -4003 | -4006 | -3999 | 0 | -1552 | -1536 | -1548 | 0 | -4633 | -4634 | 28 | 25.6 | 25.1 | 196.3 | 196.3 | 25.6 | 28 | 25.6 | 6050 | 6463 | 6588 | 7145 | 6393 | 6036 | 6429 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 854 | 2029 | 2044 | 2031 | 0 | 949 | 1118 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 949 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1073 | SUCCESS |
8993 | 9/3/2022 18:09 | 36034.49 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11581 | -4000 | -3999 | 74 | 92 | 84 | 6048 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26243 | -15126 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3877 | 3834 | 3870 | 0 | 11568 | 11544 | -4006 | -4002 | -3998 | 0 | -1553 | -1534 | -1547 | 0 | -4630 | -4634 | 28 | 25.6 | 25.1 | 196.3 | 196.3 | 25.6 | 28 | 25.6 | 6046 | 6459 | 6588 | 7145 | 6390 | 6033 | 6425 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 857 | 2029 | 2044 | 2031 | 0 | 952 | 1122 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 952 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1074 | SUCCESS |
8994 | 9/3/2022 18:09 | 36038.49 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11579 | -4000 | -3999 | 74 | 92 | 84 | 6043 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26237 | -15123 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3876 | 3833 | 3869 | 0 | 11567 | 11541 | -4005 | -4005 | -3998 | 0 | -1552 | -1535 | -1547 | 0 | -4630 | -4633 | 28 | 25.6 | 25.2 | 196.4 | 195.2 | 25.6 | 28 | 25.6 | 6042 | 6454 | 6588 | 7145 | 6386 | 6028 | 6419 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 861 | 2029 | 2044 | 2031 | 0 | 957 | 1128 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 957 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1069 | SUCCESS |
8995 | 9/3/2022 18:09 | 36042.5 | 0x0187 | 780 | 10 | 0x0081 | 0 | 65535 | 65535 | 1 | 25.6 | 11577 | -4000 | -3999 | 74 | 92 | 84 | 6039 | 6588 | 91 | 91 | 65535 | 4000 | 12300 | 0x00C0 | 14 | -26234 | -15121 | -28800 | -14400 | 93 | 0x0187 | 0x0000 | 0x04 | 0x0004 | 0xC0 | 0x0D19 | 0x03F8 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 0x0000 | 3876 | 3833 | 3868 | 0 | 11564 | 11541 | -4006 | -4001 | -4001 | 0 | -1553 | -1534 | -1548 | 0 | -4630 | -4632 | 28 | 25.6 | 25.1 | 196.1 | 196.3 | 25.6 | 28 | 25.6 | 6037 | 6448 | 6588 | 7145 | 6381 | 6024 | 6415 | -420 | -506 | 6565 | 7041 | 25.3 | 22.6 | 1000 | 1000 | 1000 | 0 | 19 | 22 | 17 | 0 | 3 | 14 | 3 | 3 | 3 | 0 | 865 | 2029 | 2044 | 2031 | 0 | 961 | 1132 | 3 | 2848 | 2800 | 2832 | 0 | 8398 | 8388 | 8404 | 0 | 2051 | 2054 | 2052 | 0 | 961 | 107 | 2.09 | 8055 | 1888 | 1856 | 1888 | 0 | 0 | 8528 | 0 | 0 | 1888 | 1856 | 1888 | 0 | 19216 | 6712 | 7322 | 1053 | SUCCESS |
Please help on the QMAX and MAXERROR update issues. Thank you!
Chen