This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: jitter

Genius 4860 points

Part Number: ISO5452

Please let us know max jitter information of this part.

1.

MAX jitter @rising edge:

MAX jitter @falling edge: 

Customer checked waveform of this part, they found about 2ns jitter.

Regards,

Kura  

  • Hi Kura,

    Thanks for your interest on the ISO5452 device.

    We do not test or have specification for rise/fall time Jitter. The spec is for Rise, Fall time for a specific load [1nF] as mentioned in the datasheet. It will be good to understand 

    whether jitter is a critical specification for your current application. Can you please share additional details?

    There are specs for prop delay for both rising (tPLH) and falling (tPHL) and also the Pulse skew spec |tPHL – tPLH|. 

    Thanks

    Sasi