Hello,
I am wondering if NXP has any LED drivers that would allow the LEDs to function with a PWM signal, as well as have fault detection to turn off all LEDs. There will be about 50-60 LEDs with a forward voltage of 3.0 v @ 30mA.
The board will only be receiving a PWM signal for dimming @ 14.5v and a ground.
If the driver needs a voltage supply (Vin), the PWM signal would have to be filtered to give a constant supply to the driver.
Needs to be automotive approved.
Thank you