Hi Team,
Our customer will use the TPS24720RGTT in aerospace project. He would like to ask for design review of their schematic diagram which I attached below.
Here are the specifications of their application.
Ambient temp, 85 deg C.
V1 = 5V @ 12A
V2 = 3.3V @ 18A
V3 = 3.3V_Aux @ 6A
CurrentLimiter_TPS24720RGTT.pdf
Initially, I noticed that the TPS24720RGTT is an industrial grade device and not for aerospace application. I also noticed that the SL1 to SL5 resistors are in 0805 package which may not be able to handle 6A, 12A ad 18A load current. Can you please confirm if there are other mistakes in the schematic diagram?
Regards,
Danilo