This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiple instances of bqWizard + USB-to-GPIO adapters on a single PC?

Other Parts Discussed in Thread: BQWIZARD, BQ78PL116

Is it possible to have multiple instances of bqWizard running on a single PC with each instance associated with a unique USB-to-GPIO probe + battery pack?

We would like to run 2 instances from a single PC if possible.

  • The bq78PL11x API was developed to allow users to create "customized" bqWizards.  This API is the source code needed to configure and calibrate the bq78PL11x devices.  See documentation on the API on the bq78PL116 product page.  There is a demo application that comes with the API that shows what is possible.  It is possible to connect multiple devices to the single application.