Part Number: DRV103
Hello E2E Experts,
Good day.
I am trying to design an economizer circuit for the main electrical contractors on my EV conversion, but I can't get the circuit to work. I followed the basic circuit diagram from the datasheet and selected the resistors and capacitors from the tables provided there.
I wanted to use a 25kHz pwm frequency, 20% duty cycle, and 110ms delay time. The system voltage is between 12v-13.5v DC. When I power up the circuit, nothing happens (the LEDs don't turn on and nothing happens when I signal the input pin on the DRV103).
I am attaching a screenshot of my KiCAD circuit. The wires going off the bottom of the screen are connecting to a second DRV103 for the second coil I am driving. Since my EV controller outputs ground to engage the contractors, I had to use a transistor and a 5v regulator to supply the 5v input signal to the DRV103.
Thank you in advance for your help.
Regards,
CSC