Hello expert,
Customer is asking for 30V~50.4V -> 12V/800W Buck controller solution. Do we have solution could meet customer's application? Thanks a lot!!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ann,
We have a 5V/50A apps circuit in the datasheet that could be adjusted for 12V/67A. However, I recommend using 3 or 4 phases, depending on max ambient temperature, as 33A/phase is a bit high with just 2 phases. Please fill out the LM5143 quickstart calculator and send me the file for review.
Regards,
Tim