Hi,
Good Day.
Customer plan on using TPS22913C but he want to select either a 3.3V output or a 5V output.
Both going on the same output, so he activate either one either the other.
He is wondering if the 5V could potentially leak back into the 3.3V.
He sent his 3.3V supply as input to one TPS22913C, he send his 5V supply as input to the other TPS22913C.
Then he connect both output together so he can feed the selected voltage to whatever is connected next.
He do have control on both "Enable" signals, so he can make sure not to activate both at the same time.
Can you make sure the 5V will not leak into the 3.3V via the TPS22913C?
Please advise. Thank you very much.
Best Regards,
Ray Vincent